Parameter and Command Error Messages
Error Message |
Meaning |
Remedy |
Occurrence |
---|---|---|---|
Error: Parameter or command was not found. |
Parameter or command string was not recognized as a known command. |
Check the entered string for accuracy. Consult the reference guide or enter DRV.LIST in the WorkBench terminal screen to find valid parameters and commands. |
General. |
Error: Not a trigger parameter. |
Parameter cannot be used for triggering the scope. |
Use a different parameter as a trigger value. |
Recorder parameters. |
Error: Parameter not recordable. |
Parameter cannot be scoped. |
Do not scope this parameter. |
Recorder parameters. |
Error: Wrong argument for parameter or command. |
Argument was not accepted. |
Check the entered argument for accuracy. Consult the reference guide or enter DRV.LIST in the WorkBench terminal screen to find valid parameter and command arguments. |
General. |
Error: No arguments allowed for parameter or command. |
Parameter or command supports no arguments. |
Enter parameter or command again with no arguments. |
Commands and read-only parameters |
Error: Too many arguments for parameter or command. |
Too many arguments provided for this parameter or command. |
Enter again with fewer arguments. |
All parameters and commands with no or one argument. |
Error: No float allowed. |
Float number was entered, but only integer numbers are allowed. |
Enter integer value instead. |
All parameters and commands with integer arguments. |
Error: Parameter or command is read-only. |
Argument was not accepted because the parameter or command is read-only. |
Enter again with no arguments. |
Commands and all read-only parameters. |
Error: Parameter is temporarily write protected. |
Argument was not accepted because the parameter is currently read-only. |
Check reference guide or KAS IDE |
Some parameters that come from the Smart Feedback Device |
Error: Argument greater than maximum value. |
Entered argument was beyond maximum value. |
Enter a value that is within the allowable range. See reference guide or KAS IDE help for ranges. |
Commands and read-write parameters. |
Error: Too many characters in parameter or command. |
Parameter or command string was too long. |
Shorten string and enter again. |
General. |
Error: Argument less than minimum value. |
Entered argument was too small. |
Enter value that is within the limits. |
Commands and read-write parameters. |
Error: Argument is out of data range. |
Entered argument was not withing the data range limits. |
Enter value that is within the limits. |
Commands and read-write parameters. |
Error: Parameter or command is password protected. |
Use of this parameter or command requires a password. |
Contact technical support to obtain password. Enter valid password. |
Password protected parameters and commands. |
Error: Wrong operation mode for parameter or command. |
Requested parameter or command cannot be performed in this operation mode. |
Change to valid operation mode. |
|
Error: Drive enabled. Disable drive and continue. |
Action can only be performed if drive is disabled. |
Disable drive and repeat action. |
|
Error: Drive disabled. Enable drive and continue. |
Action can only be performed if drive is enabled. |
Enable drive and repeat action. |
|
Error: Data value is invalid. |
Entered data was not valid. |
Provide valid data. |
|
Error: Argument must be an even number. |
Argument is not an even number. |
Enter a value divisible by two without remainder. |
|
Error: Argument must be an odd number. | Argument must be an odd number. | Enter a value not divisible by two with remainder. | |
Error: Axis is not homed. |
Axis is not homed. |
Home axis and repeat action. |
|
Error: All recorder channels empty. |
No data is specified to record. |
Specify the data to be recorded and start again. |
Recorder commands. |
Error: Process already active. |
Required action is already running. |
Wait until action is finished and start again if needed. |
|
Error: Motor is currently in motion. |
Action can only be performed if motor is not moving. |
Stop motion and repeat action. |
Motion tasks, service motion, and others. |
Error: EEPROM is bad or does not exist. |
EEPROM is damaged. |
Restart drive. If fault persists, replace the drive and consult technical support. |
|
Error: Unknown board. |
|
|
|
Error: Fault exists.Correct fault condition and then clear faults. |
A fault is present in the system. |
Clear the fault, disable the drive, and then enable the drive again. |
|
Error: Cannot clear faults. Issue software or hardware disable first. |
|
Clear hardware or software enable and repeat action. |
|
Error: EEPROM is busy. |
|
|
|
Error: Invalid motor/feedback poles ratio. |
|
|
|
Error: Unknown Fault. |
Situation should not happen. |
Clear fault. If fault recurs, consult technical support. |
Unknown. |
Error: Invalid motion task velocity. |
Motion task velocity is zero. |
Use a non zero velocity value. |
Setting up a motion task. |
Error: Invalid motion task following number. |
Motion task index for following motions task is invalid. |
Use a valid motion task index. |
Setting up a motion task. |
Error: Function |
Operionation cannot be performed using the current commad source. |
Change the command source to executue the operation. |
Various funtions (homing, Electronic Gearing, motion tasking, service motion). |
Error: Not enough memory available. |
Cannot allocate flash memory. |
Power cycle the drive and try again. If problem persists, contact Customer Support. |
Functions that access flash memory. |
Error: Buffer overflow. |
Could not fit data into allocated buffer. |
Power cycle the drive and try again. If problem persists, contact Customer Support. |
Functions that communicate with safety devices and flash. |